Table Diagnostics
This display provides database table diagnostics and allows to monitor table sizes and splits of tables.
Database Tables
| Property Name | Data type | Description |
|---|---|---|
| Name | String | Name of database table. |
| Size On Disk | Single | Size of the table in disk. |
| Is History | Boolean | If selected, table is historized. |
| Splits | UInt16 | Shows number of splits. |
| Is Deleted | Boolean | If selected, table has been deleted. |
| ComputerName | String | Shows the node name. |
Chart
When table is selected from datalist (pressed as active), the chart below shows Size on Disk and amount of Splits in chart. Time bar below allows to change the shown time period and allows to scroll back in history.

Updated about 2 months ago
Did this page help you?