Package manager based installation
While on Linux the package manager based installs are a standard way of installing software, on Windows it is not so common. Since version 5.2, ABB Ability™ History now has experimental support for the package manager based install also on Windows. This support is currently based on Chocolatey.
Please Note As the package managed-based installation support is still experimental, it is recommended currently to try it only in a system that can be wiped afterward, e.g., inside a virtual machine
Preparations
The package managed based installation method relies on Chocolatey, which is a package manager for Windows. You can follow this guide to install Chocolatey.
When you have Chocolatey installed, then add the ABB Ability™ History repository.
choco source add -n cpmPlus -s http://cpmplus-repository.abb.com:5001/ --bypassproxyInstallation
To view the packages in the ABB Ability™ History repository, try:
choco search cpmPlusIn order to install something, such as cpmPlusHistoryMono, try:
choco install cpmPlusHistoryMono_x64Updated over 1 year ago
Did this page help you?