Using VtrinCmd as the Import Tool
This document contains examples for importing data with VtrinCmd.
For more information about connecting to a data source, connection types, credentials, and command parameters, see the VtrinCmd Tool documentation.
Parameters
| Command | Description |
|---|---|
| --connectionstring | Database Connection |
| --importjson | Import JSON data from a file(s). Multiple files separated with | |
| --importjsonfolder | Import data from .json files in a folder recursively. Folder path as parameter. |
Import a single JSON file
VtrinCmd --connectionstring /path/to/your/data --importjson "path-to-file.json"
Importing Multiple Individual Files
To import multiple JSON files in a single command, use the | separator.
VtrinCmd --connectionstring /path/to/your/data --importjson "path1|path2"
Import a Folder
To import all JSON files from a folder and its subfolders.
VtrinCmd --connectionstring /path/to/your/data --importjsonfolder "path-to-folder"
Note: --importjson can also be given a folder path. In this case, VtrinCmd will ask for confirmation (y/N) before importing, to prevent accidental bulk imports.
Further Reading:
Learn more about VtrinCmd tool
Updated 2 days ago
Did this page help you?