Status property icons
Status property of CurrentValue
The VtrinLib CurrentValue class presents the status information only with an unsigned 64 integer bitmask number. C# programs that have access to VtrinLib can interprete this with the following enum definition in namespace ABB.Vtrin.
cValueStatus Enumeration
| Icon | Name | bitmask number | Description |
|---|---|---|---|
| OK | 0x0000000000000000UL | Status indicating that current value status is okay and value is good quality. | |
| ManuallySet | 0x0000000000000100UL | Status for value that has been manually set. | |
| Increasing | 0x0000000000000200UL | Status indicating that current value has increased from previous value. | |
| Decreasing | 0x0000000000000400UL | Status indicating that current value has decreased from previous value. | |
| StartOfSlice | 0x0000000000000800UL | Filter type status that is used when referred to starting time of a certain time period (E.g. start time when engine was running). | |
| EndOfSlice | 0x0000000000001000UL | Filter type status that is used when referred to ending time of a certain time period (E.g. end time when engine stopped running). | |
| Interpolated | 0x0000000000002000UL | Status indicating that there is an interpolated value in between two real history values. | |
| Extrapolated | 0x0000000000004000UL | Status indicating that an extra value is added after a certain history time period. May be described as prediction value. | |
| Fake | 0x0000000000006000UL | Created value to history that has not been created naturally. Fake value could be added e.g. through a filter. | |
| LastInSequence | 0x0000004000000000UL | Status that indicates last value of a time period. Data collection ends and the value expires at this point. | |
| HistorySubstituted | 0x0000008000000000UL | Status related to history maintenance. Indicates that a value in history has been fixed or overwritten. Calculation cannot overwrite this HistorySubstituted value. | |
| Uninitialised | 0x0000020000000000UL | Status to indicate a value that only a filter could produce. | |
| AccessDenied | 0x00000A0000000000UL | Displayed when user does not have right to access value information. | |
| Frozen | 0x0000100000000000UL | Status indicating that a value has been frozen or locked. Prevents overwriting the value. Weaker than HistorySubstituted. | |
| Incomplete | 0x0000200000000000UL | Status indicating that current value is imperfect. | |
| Substituted | 0x0000800000000000UL | Value has been overwritten, could be manually set. | |
| SupressedAlarm | 0x0001000000000000UL | Status indicating an alarm that has been supressed. Includes InformativeAlarm, WarningAlarm,ErrorAlarm and CriticalAlarm. Icons are on table below. | |
| Questionable | 0x0002000000000000UL | Status indicating that current value is not defined yet or cannot be sure of the quality the value. | |
| AlarmLevel | 0x0FFC000000000000UL | Status indicating that current value has reached level that has raised alarm. Includes statuses InformativeAlarm, WarningAlarm,ErrorAlarm and CriticalAlarm. | |
| Bad | 0x1000000000000000UL | Status shown when producer of current value indicates the value is broken. | |
| Disabled | 0x2000000000000000UL | Status indicating that current value has been disabled. | |
| Invalid | 0x4000000000000000UL | Current value is not set or the value is otherwise invalid. |
Example for updating value with timestamp and status
Below is an example for updating property value with timestamp and status. The update is done through CurrentValue table.
cDbClassInstance instance = GetDriver().Classes["Path"].Instances.GetInstanceByName("My New Instance");
object property = GetDriver().Classes["Path_My Equipment Type"].GetProperty("My New Property").GetLowLevelValue(instance);
cDbClassInstance tempInstance = GetDriver().Classes["CurrentValue"].Instances[property].BeginUpdate();
tempInstance.Value = 8;
tempInstance.TimeUTC = DateTime.UtcNow.AddDays(-5);
tempInstance.Status = cValueStatus.Fake;
tempInstance.CommitChanges(true);
cValueStatusResolved Enumeration
| Icon | Name | Value | Description |
|---|---|---|---|
| NoStatus | -1 | No status available for current value. | |
| OK | 0 | Status indicating that current value status is okay and value is good quality. | |
| Substituted | 1 | Value has been overwritten, could be manually set. | |
| SupressedInformativeAlarm | 2 | Information alarm, that has been supressed. | |
| SupressedWarningAlarm | 3 | Warning alarm, that has been supressed. | |
| SupressedErrorAlarm | 4 | Error Alarm, that has been supressed. | |
| SupressedCriticalAlarm | 5 | Critical alarm, that has been supressed. | |
| Questionable | 6 | Status indicating that current value is not defined or cannot be sure of the quality of the value. | |
| InformativeAlarm | 7 | Information type alarm. Does not necessarily require action. | |
| WarningAlarm | 8 | Alarm for warning. | |
| ErrorAlarm | 9 | Alarm for errors. | |
| CriticalAlarm | 10 | The highest and most severe alarm.Indicates system is down. | |
| Invalid | 11 | Invalid current value. | |
| Uninitialized | 12 | Known value has not been given. |
Updated 7 months ago
Did this page help you?