Service configuration on systemd
The RTDB services are managed with the RTDB service manager, which is handled by systemd. Other processes are not seen as service for the Linux system.
Create database
In case you need to create a new database, it can be achieved using the following command:
RTDB_Create_New_Database /path/to/databaseDatabase scan
To initialize the database on the Linux system, you need to scan the database. To scan the database, run the command below.
RTDB_ScanDB -abp /path/to/database '*'Service configuration
Run the following commands to install the services needed. Note that when calling "systemd enable", you need to replace the slashes with hyphens.
Common services
RTDB_CVMCServer -install /path/to/database
RTDB_Transformator -install /path/to/database
RTDB_Scheduler -install /path/to/databaseVtrin-NetServer
Vtrin-NetServer is added as a service with CSCommon_CMD.
CSCommon_Cmd -setini /path/to/database/RTDB.INI Services Vtrin-NetServer ON
CSCommon_Cmd -setini /path/to/database/RTDB.INI Vtrin-NetServer BinaryPath "mono /usr/share/cpmplus/mono/Vtrin-NetServer.exe -d" #for monoSystem monitor
System Monitor is installed with the install flag. Pick one line below depending on what version you have downloaded (mono or core version).
#For Mono
sudo mono /usr/share/cpmplus/mono/RTDB_SystemMonitor.exe --install -databasepath /path/to/database
# For .NETcore
sudo dotnet /usr/share/cpmplus/netcore/RTDB_SystemMonitor.dll --install -databasepath /path/to/databaseStarting services
Services are started with the command:
systemctl enable rtdb@/path/to/database
systemctl start rtdb@/path/to/database
In case of getting error "Failed to enable unit, file rtdb@/path/to/database: Invalid argument.", try formatting path in following way.systemctl enable rtdb@-path-to-database
Reading service logs
You can view the service logs by the following command.
journalctl -r -u [email protected]Updated over 1 year ago