Internal Events

OPC Events and external events, as described in External events, provide means to store events collected from any third-party system that supports the OPC A&E server interface. Contrary to this, internal events are events that are generated based on numerical data collected to RTDB. Event generation is controlled by creating event triggers ("EventTrigger" Vtrin class, or "Event definition" in user interfaces). The following sections give detailed information on how to use and understand available events, as well as how to create new event triggers to spawn new internal events.

Event triggers are configured for database variables. The system uses event triggers to generate events with different severities (critical alarms, warnings, notices, and non-alarms) when the conditions that have been specified for the triggers are fulfilled. Typical triggers for analog variables are high limits and low limits. Typical triggers for binary variables are state changes.

For example, a high limit trigger would let the system generate an event of a certain severity when the value of the variable exceeds the high limit. Another event might be configured to be generated when the value returns below the high limit.

The following figure illustrates the logical relationships between related classes.

Event triggers are created using the "Event Configuration" list available from Vtrin in Maintenance\System\Events and Alarms. The "Event Configuration" list is a master-detail list where variables, which have event triggers associated, are presented in the upper part. The event trigger associated with a particular variable is shown in the lower part when the variable is selected in the upper part. After installation, there are no event triggers available, and the display is empty.

For example, a row could define that a warning event is triggered when the value of the variable specified on the row becomes higher than the limit specified on the row.

To be able to configure events, write access is needed to the database.

The easiest way to create event triggers is by using Vtrin. The "Event Configuration" list is found from the main tree in Maintenance\System\Events and Alarms. In the following example, a new variable, "EventTriggerTestVariable" is created. It is used to generate events whenever the current value of the variable becomes greater than 10.

  1. A new variable is created from the upper part of the "Event Configuration" display. If a variable is created from this display, the value of the "Events" property is automatically set to "true". If an existing variable is used, this should be set to true manually (this has to be done from the list view or from the generic properties, as the property is not available in the custom variable dialog).
  2. A new event trigger is created from the lower panel (from "Edit mode", click the "New" button). The property "InUse" should be set to "true". The limiting trigger value 10 is configured to the property "Limit" (by default, the "TriggerType" is already "High limit"). Finally, the value of the "Log" property is set to "true". This enables logging into the "Alarm log". In case the value of the "Log" property would be "false", the warning would only be visible from the variable instance's blinking current value with an appropriate warning icon. Changes are committed using the "Commit" button, and after that returning from "Edit mode" to "Normal mode" (Revert).
  3. Testing the configuration can be done by double-clicking the variable and feeding a value bigger than 10 for the current value.

The following figure illustrates the situation after the three steps above are executed.

EventEngineering Attributes (RTDB Core)

AttributeTypeDescription
Variable (IDN)uint32Reference to the variable instance where the event trigger is applied.
PathIdGUIDHierarchical path to the variable.
PropertyIdGUIDIdentifier of the property definition on the variable instance to which the event trigger is attached.
ReferenceInstanceGUIDIdentifier of the specific object instance that the trigger’s reference points to
ReferencePropertyGUIDIdentifier of the property definition on the referenced instance whose value is used by the event trigger.
EERbinaryCombines in binary format all the other attributes except IDN.
Descriptionstring[64]Description of the variable where the event trigger is applied.
InUseboolTrue if the trigger will be evaluated, false if not.
EventTriggerIdGUIDID of the event trigger
Triggeruint32Read the next chapter for more detailed value descriptions.
TriggerCauseuint32Why the trigger actually fired
LimitobjectDefines the limit that causes the state transition in event triggering. The type is derived from the variable instance"s type, and can be either 64bit integer or double.
NOTE: if low level access (e.g. RTDB Core ODBC) is used for writing the value, the data type must be Int64 or Double. When written via VtrinLib, the data type will automatically be corrected if given differently.
Formatuint32Output format for trigger
ReturnFormatuint32Output format for return
PerioddoubleTime period in seconds, if the event or limit value represents some time-dependent value.
Areauint64Defines which alarm area the event trigger belongs to. The numeric value should not exceed 65535 because the value in AlarmLog is only 16 bits. If the setting is zero, the ProcessArea from the alarming Variable or Equipment property is used instead. (Version info: before 5.1/2017-04-25, the setting was ignored and worked as it was given as zero).
DeadBandobject (float/int)After some state change has been triggered, the return back to normal state happens once the limit has been (strictly) exceeded with the specified dead band. The dead band is absolute (and not relative to measurement limits).

The dead band is inclusive, so that for example, with high limit, the value must decrease strictly below the value "Limit-DeadBand" in order to inactivate the alarm (the alarm will not inactivate yet if the value drops exactly to "Limit-DeadBand"). The main reason for this is that then the default dead band of zero works sensibly for analog measurement values that for example vary between 10.0049 and 10.0051 but for tecnhical reasons is rounded to nearest 0.01 units. It would not make sense that the alarm would be deactivated on each change from 10.01 to 10.00 and then alarm created again when the value changes from 10.00 to 10.01.

A negative value (-1 is recommended) can be used to disable the deadband handling completely (but see version info below).

NOTE: if low level access (e.g. RTDB Core ODBC) is used for writing the value, the data type must be Int64 or Double. When written via VtrinLib, the data type will automatically be corrected if given differently.

(version info: disabling the deadband needs version 5.3_26.08. Previously it was not specified what negative value means. For integer variables the value -1 actually could be used to effectively disable the deadband with integer variables. See also release notes of WI#72368).
Externaluint32External event observation identification. If EventEngineering.External is greater than 0, the event observation, or limit handling, for the event is performed by the source of the value (e.g. an external data acquisition system). The event identification is provided in the latest value attribute CLEX (=EventEngineering.External), if the event is triggered (limit violated) and it has higher priority than the other external events.
Referenceuint32In addition to using a static limit, there is the possibility to use another variable's value as a dynamic limit. "Reference" is set to contain a reference to the variable that contains the current value to be used as the dynamic limit.
TriggerMethod(TriggerM)uint32In case the "Trigger" is 13 ("Event trigger method"), the "TriggerMethod" defines the method that is used to evaluate the trigger condition. If the method returns true, the event state is valid.
SuppressionMethod(SuppressionM)uint32Alarm suppression method. If the conditions for the event are fulfilled, but the method execution specified by EventEngineering.SuppressionM returns a nonzero value, the specified alarm (EventEngineering.Priority) is suppressed. An indication for the suppressed alarm is set (CSAS). The event observation is continued. The special suppression method is AlarmSuppressed (11), which means that the alarm is suppressed without executing any other method.
ActionMethod(ActionM)uint32Action method to be executed when entering the event state. If EventEngineering.ActionMethod is zero, no method is executed. EventEngineering.ActionM is a user-written method.
ReturnMethod(ReturnM)uint32Action method to be executed when leaving the event state. If ReturnMethod is zero, no method is executed. ReturnMethod is a user-written method.
DiaryboolIf true, event is stored into diary log if available.
LogboolIf true, event is stored into alarm log.
OpcEventboolIf true, event is stored into Opc Event log. (From Version: 5.3/2022-12)
DiaryReturnboolIf true, event from returning back to normal state is stored into diary log.
LogReturnboolIf true, event from returning back to normal state is stored into alarm log.
OpcEventReturnboolIf true, event from returning back to normal state is stored into Opc Event log. (From Version: 5.3/2022-12)
TransitionAlarmboolCan be used together with the change limit triggers to immediately inactivate the alarm without waiting for the next cyclic processing to inactivate the alarm. The "LogReturn" setting is not applicable togther with TransitionAlarm. TransitionAlarm should be used only for change limit triggers. Otherwise there will typically be repeated alarms.
(Version info: 5.3_26.10)
SetQuality (Set Validity)uint2Status that the system sets for the variable when the triggering condition becomes true ("No change", "Set questionable", "Set bad").
Evaluationuint8If the variable has several event triggers, the "Evaluation" defines the priority that the triggers are evaluated by.
Priorityuint8Alarm priority used when condition is triggered.
ReturnPriorityuint8Alarm priority used when returning back to normal state.
ModifiedDateTimeRow modification time shows the last time when the event trigger instance has been modified.
RowModificationTimeDateTimeLast modification timestamp (local time)
RowModificationTime_UTCDateTimeLast modification timestamp (UTC)
SpeakboolIf a sound-support package has been installed, the events generated are spoken.
EvaluateAlwaysboolThe system checks this trigger always even if an earlier trigger is active, so that multiple triggers can be active for the same variable. Notice that when multiple alarms are active, the "Alarm Priority" information of the current value describes the priority of the active alarm with highest priority. The active alarms can be found from the ActiveAlarm class (ActiveAlarms database table), from entries where the "IsActive" property is true (version info: 5.3_25.06)
(version info: before 5.3_26.06, the highest evaluation order setting defined the alarm priority of the variable)
EvaluateAlsoForInvalidboolEvaluate this trigger also if the current value was invalid. Without this, most triggers evaluate only for valid current values. (version info: 5.3_25.06)
EvaluationConditionVariableuint32

VariableId of a Variable whose value defines the condition to evaluate this trigger.

If non-null, the value of this variable must be in the set of Condition Flags of property EvaluationConditionValue to enable evaluation of this trigger. This property together with the EvaluationConditionValue property can be used to implement "Plant Mode" specific triggers.

The plant modes are integer values between 0 and 9. (Values up to 30 can be used but only the first 10 has been declared in UIStrings as Flags to be used in EvaluationConfitionValue).

For example, if the EvaluationConditionValue is 48, it means that this trigger is evaluated if the plant mode is currently 4 or 5 (i.e. 2^4 + 2^5 = 16 + 32 = 48).
The user interface presents the EvaluationConditionValue as a "flags" style enumeration, so that the user does not need to perform the above calculations, but can just define the settings as "M4 | M5" (I.e. for plant mode 4 and 5).

Notice that in many cases a site has only one plant mode variable, but the configuration supports multiple of them because the setting is trigger definition specific. (version info: 5.3_25.06)

EvaluationConditionValueint32Set of Condition flags. Multiple settings can be entered separated with pipe character (|). See description of "EvaluationConditionVariable". (version info: 5.3_25.06)
AutomaticAcknowledgeboolWhen the event triggers, the alarm is automatically defined to be already acknowledged. (version info: 5.3_26.06)
ManualAlarmSuppressionboolThe trigger is manually suppressed. This has the same effect as setting the SuppressionMethod to "Alarm suppressed". The purpose of this separate setting is that that the operator can quickly suppress the alarm without need to remember what was the original setting of SuppressionMethod
(version info: 5.3_26.06)
RecommendedActionuint32Recommended action when the event is triggered. Enumeration named 'Event Trigger Recommended Actions'. (version info: 5.3_26.09)
TrailLogEnableboolA TrailLog entry is written when the trigger activates. See also TrailLogPastDuration and TrailLogFutureDuration. The PathId of the Variable or Property goes to the PathId of the TrailLog. This means that the Variables that have this PathId (or its descendant) will be saved to Trail data.

The "HistoryId" in the TrailLog is stored as null, which means that all history tables that have TrailEnabled as true in the history definition are included (notice that by default, none are).

There is experimental support for storing the TrailLog columns TriggerType, TriggerName and to override the PathId setting. Ask the engineering support if you need to configure these (hint for the engineering support: See the integration test program "EventEngineeringTest.TrailLog" for an example).
(version info: 5.3_26.10)
TrailLogPastDurationdoubleNumber of seconds to the past direction from the event time to be used as the TrailLog StartTime. (version info: 5.3_26.10)
TrailLogFutureDurationdoublleNumber of seconds to the future direction from the event time to be used as the TrailLog EndTime. (version info: 5.3_26.10)
TrailLogHistoryIduint32The Id of the history table to be selected for Trail storing. Zero means that all history tables are included that have TrailEnabled.

Type Enumeration of Event Trigger

ValueDescription
  1. High limit
Triggers when the value of the associated variable exceeds the value in the "Limit" property.
  1. Low limit
Triggers when the value of the associated variable goes below the value in the "Limit" property.
  1. Change speed limit
The maximum change per time period (the time period defined in "Period"), and the limit value is "Reference" or "Limit". Valid only for double type variables.
  1. Difference limit
The maximum difference to the reference variable ("Reference"). Valid only for double type variables.
  1. Total match
To detect binary value states. Triggers when all bits match. Valid only for int64 and binary type variables.
  1. Any bit match (bitwise AND not zero)
To detect binary value states. Triggers when any bit matches. Valid only for int64 and binary type variables.
  1. Oscillation surveillance
If the value of the binary point changes more than once within the specified time period ("Period"), the event is generated. Valid only for int64 and binary type variables.
  1. In-transit state surveillance
If the state change of a two or four signals digital input value has taken more than the specified time period ("Period"), the event is generated. Valid only for binary type variables.
  1. Binary indicated limit violation
Indicated by a separate binary variable specified in the "Reference" property. When the binary goes to 1, the event is triggered. "Reference" defines the limit indicator binary for the analog variable, and the corresponding analog variable for the binary indicator.
  1. Expiration surveillance
If the time since the last update (CLT) of the variable is longer than defined in the period ("Period"), an event is generated.
  1. Disabled processing surveillance
If the current value processing of the variable is disabled (EGE=false), an event is generated.
  1. Bad measurement group surveillance
If the latest value has "bad measurement group" status (CLSBG), an event is generated.
  1. Bad value surveillance
If the status of the latest value is "bad" (CLSB), an event is generated.
  1. Trigger condition method
User-written trigger method ("TriggerMethod") is used as a trigger condition. Note: the actual implementation is not documented yet in detail.
  1. Pulse input power surveillance
Time derivation aggregate is decreased, if a new pulse value has not been produced in the time interval defined in "Period".
  1. Reset reference variable
Set the value of the "Reference" variable to zero, when the state changes to binary value on (1). This trigger is only valid for binary variables. The event does not stay valid and it does not cause the event actions, event logging, or alarm priority changes.
  1. -22.
Reserved for RTDB_GradeServer use.
  1. Change limit, absolute
Triggers when the value changes more than the given absolute limit. Deadband is taken into account.
  1. Change limit, signed
Triggers when the value changes more than the given signed limit (grows if positive or decreases if negative). Deadband is taken into account
  1. Value range violation
Triggers when the value is outside of the measurement range
  1. Limit clamping to measurement range
Triggers when the value is outside the measurement range and substitutes the value with the min or max value respectively.

EventTrigger Attributes for Variables (VtrinLib)

NOTE: For more detailed description of the attribute, see the chapter "EventEngineering Attributes (RTDB Core)" above.

ColumnTypeDescription
IdGUIDUnique event trigger identifier
Variableuint32Variable ID this trigger applies to
DescriptionstringVariable description
InUseboolTrigger enabled
PerioddoubleTime period in seconds
Areauint64Alarm area identifier
Externaluint32External event handler ID
Referenceuint32Reference variable (dynamic limit)
ReferenceInstanceGUIDReferenced instance
ReferencePropertyGUIDReferenced property
Triggeruint32Trigger type (limit, state, method, etc.)
TriggerCauseuint32Cause code of trigger activation
Limitobject (double or int64)Trigger limit value
DeadBandobject (double or int64)Deadband for return to normal
TriggerMethoduint32Trigger evaluation method
SuppressionMethoduint32Alarm suppression method
ActionMethoduint32Method executed on trigger
ReturnMethoduint32Method executed on return
Priorityuint32Alarm priority
ReturnPriorityuint32Priority on return
SpeakboolText-to-speech enabled
DiaryboolLog event to diary
LogboolLog event to alarm log
OpcEventboolGenerate OPC event
DiaryReturnboolLog return event to diary
LogReturnboolLog return to alarm log
OpcEventReturnboolOPC event on return
TransitionAlarmboolCan be used together with the change limit triggers to immediately inactivate the alarm without waiting for the next cyclic processing to inactivate the alarm. The "LogReturn" setting is not applicable togther with TransitionAlarm. TransitionAlarm should be used only for change limit triggers. Otherwise there will typically be repeated alarms.
(Version info: 5.3_26.10)
SetQualityuint32Quality state to set
Evaluationuint32Evaluation mode
EvaluateAlwaysboolAlways evaluate trigger
EvaluateAlsoForInvalidboolEvaluate even if value invalid
EvaluationConditionVariableuint32Conditional variable ID
EvaluationConditionValueint32Conditional comparison value
Modified_UTCdatetimeLast modification timestamp
TriggerDescriptionstringHuman-readable trigger text
AutomaticAcknowledgeboolWhen the event triggers, the alarm is automatically defined to be already acknowledged. (version info: 5.3_26.06)
ManualAlarmSuppressionboolThe trigger is manually suppressed. This has the same effect as setting the SuppressionMethod to "Alarm suppressed". The purpose of this separate setting is that that the operator can quickly suppress the alarm without need to remember what was the original setting of SuppressionMethod
(version info: 5.3_26.06)
RecommendedActionuint32Recommended action when the event is triggered (version info: 5.3_26.09)
TrailLogHistoryHistoryReference to the history table to be selected for Trail storing. Null ("None") means that all history tables are included that have TrailEnabled.
Other TrailLog propertiesSee description in the previous section for RTDB Core EventEngineering table attributes.

Equipment Model Event Triggers

It is possible to trigger events when a specific property on an equipment instance changes. This is done using the EventTriggerEquipmentProperty class (the class name is "Event definition for Equipment Property" in user interfaces).

1662

A conceptual model that shows how event triggers are related to the equipment model.

There are three ways of how property events can be set to trigger:

  1. When the property of a specific instance changes
  2. When the property of any instance of a specific equipment type changes
  3. When the property of any instance of a specific equipment type under a hierarchy subtree changes

From a configuration perspective, 1. and 2. are just special cases of 3. In 1., the subtree contains just the one instance and in 2., the subtree equals the whole hierarchy.

EventTriggerEquipmentProperty Attributes (VtrinLib)

NOTE: For more detailed description of the attribute, see the chapter "EventEngineering Attributes (RTDB Core)" above.

ColumnTypeDescription
IdGUIDUnique identifier of the event trigger.
InstanceGUIDEquipment instance to which the trigger is applied.
PropertyGUIDProperty definition on the equipment instance being monitored.
Triggeruint32Trigger type enum that defines how the event condition is evaluated.
InUseboolEnables or disables the trigger.
Limitobject (double or int64)Limit value used by limit-based triggers. Data type must match the monitored property type.
DeadBandobject (double or int64)Deadband used for return-to-normal evaluation.
PerioddoubleTime period in seconds for time-dependent triggers.
Priorityuint32Alarm priority when entering the event state.
ReturnPriorityuint32Alarm priority when returning to normal state.
Areauint64Alarm area identifier.
Externaluint32External event observation identifier. Zero means internal handling.
Referenceuint32Reference variable or identifier used for dynamic limits or comparisons.
ReferenceInstanceGUIDTarget instance providing the referenced value for dynamic or reference-based triggering.
ReferencePropertyGUIDProperty on the referenced instance whose value is used by the trigger.
TriggerMethoduint32Method used to evaluate the trigger when method-based triggering is configured.
SuppressionMethoduint32Method used to suppress alarms when conditions are met.
ActionMethoduint32Method executed when entering the event state.
ReturnMethoduint32Method executed when leaving the event state.
DiaryboolIf true, the event is written to the diary log.
LogboolIf true, the event is written to the alarm log.
OpcEventboolIf true, an OPC event is generated on trigger activation.
DiaryReturnboolIf true, a diary entry is written on return to normal.
LogReturnboolIf true, an alarm log entry is written on return.
OpcEventReturnboolIf true, an OPC event is generated on return to normal.
SetQualityuint32Quality value to set when the trigger activates.
Evaluationuint32Evaluation mode controlling how trigger conditions are processed.
EvaluateAlwaysboolIf true, the trigger is evaluated continuously.
EvaluateAlsoForInvalidboolIf true, the trigger is evaluated even when the property value is invalid.
EvaluationConditionVariableuint32Variable or identifier used as an additional evaluation condition.
EvaluationConditionValueint32Comparison value for the evaluation condition.
SpeakboolEnables speech output when the event is triggered.
TriggerDescriptionstringHuman-readable description of the trigger, mainly for UI and diagnostics.
RecommendedActionuint32Recommended action when the event is triggered (version info: 5.3_26.09)

Did this page help you?