View Dashboard important components and Context
-
Dashboard: A Dashboard is for integrating and coordinating visualization with widgets, context management, and data processing. Key features of dashboard include:
- Context Builders: Configure context listeners for managing data and interactions.
- Handlers: Process incoming context.
- Nested Dashboards: Enable dashboards to include other dashboards as widgets.
- Widget Context Management: Each widget can emit, listen, and process context using its internal logic.
- Data Source Integration: Widgets are connected to Database for real-time data retrieval and processing.
-
Widgets: Visualization Components:
Visualization Types:- Chart: Retrieves and displays time-series data between a selected Start Time and End Time, based on the Time Bar Widget.
- Pie Chart: Represents proportional data from selected time intervals or categories.
- Gauge: Displays live measurements.
- Label: Shows text.
- Value Widget: Retrieves and displays the Current Value/Historical value.
Interaction with Data Sources:- Widgets can connect to the Database, retrieving data in real-time or historical data for visualizations. Example:
- A Chart fetches historical data using a Start Time and End Time provided by the Time Bar Widget.
- Value Widget displays the current value/historical value of a variable or equipment property based on configuration
- Widgets can connect to the Database, retrieving data in real-time or historical data for visualizations. Example:
-
Context Builders – In the dashboard properties this is a section
Configure Context Listeners, which include:- Widget: Represents a specific visual component.
- Context Key: A unique identifier for context.
- Handling Dropdown: Defines context sources:
- External: Sends context to external dashboards.
- Local: Sends context within the same dashboard.
- Both: Sends context from both sources.
-
Context Mapper– In the dashboard properties this is a section
- Facilitate the processing of incoming context from other dashboards or from widgets also.
- Configure Handlers, which include:
- Key: Identifies context to process.
- Class (Data Source): Represents the source for context handling.
- Target Reference: Specifies the target widget, this is where the context will be used.
-
Widget Level Context Management:
- Unique Context Key::
- Each widget must have a unique context key for precise identification.
- Widget Context Emission::
- Widgets can emit their own context during runtime or on dashboard initialization.
- Widget Context Listening and Handling:
- Widgets dynamically process incoming context using internal logic to:
- Update visualizations (e.g., adjust time ranges on a Chart).
- Perform actions (e.g., update parameters on a Gauge or Label).
- Unique Context Key::
-
Global Context:
- Send Global Context:
- Broadcast context globally for cross-dashboard interactions.
- Listen Global Context:
- Subscribe to global context for system-wide event handling.
- Send Global Context:
-
Nested Dashboards:
- Nested dashboards can:
- Emit Context: Propagate context to parent dashboards or other widgets.
- Listen to Context: Subscribe to local, external, or global context.
- Nested dashboards can:
-
Inter-Widget Context Listening:
- Avoid Circular Reference:
- Maintain a hierarchical structure to prevent loops between widgets or dashboards.
- Widgets Interact Dynamically:
- For example, a Select Widget sends Source and selected Process path as a context:
- A Label widget show the process path selected in the Select Widget when Label Widget Listen to Context (of Select widget).
- For example, a Select Widget sends Source and selected Process path as a context:
- Avoid Circular Reference:
Updated about 1 year ago
Did this page help you?