Filters
Concept
Filtering is a mechanism to further process raw time series data. It is used by typing in the keywords defined in the filter syntax. The syntax and keywords are described in the following article.
The syntax consists of a filter selection part and the time period part. For example "AVG10MIN" calculates and shows the averages over ten minute time spans. Several filters can also be applied on top of each other. They are separated with pipe '|', for example "AVG1MIN|MAX1H" produces the hourly maximum values from the one minute average values.
In case aggregated histories are collected for the used raw time series data, filters are able to automatically use it to optimize the calculation In case optimization is not wanted to happen, it can be set off by starting with an empty filter, that is pipe '|'. For example: "AVG1MIN" is optimized while "|AVG1MIN" is not optimized.
Filters can be used from GLOSSARY:ENGINEERING UI trend or from any program using Vtrinlib API. As well OData and ODBC provides filters as is. OPC UA and HDA Servers implement HA Aggregates which are close relatives to filters only difference being the fact that aggregations can't be stacked on top of each other.
Please find further information on how to use filters with graphs under Time Series > Aggregates and filters.
Supported filters
| Filter name | Description |
|---|---|
AAVG |
Arithmetic Average |
AAVGRAW |
Arithmetic Average including invalid values |
ADEV |
Arithmetic Deviation |
ADEVP |
Arithmetic Deviation of Entire Population |
AMAX |
Arithmetic Maximum of valid values. (version info: 5.3_24.12) |
AMEDIAN |
Arithmetic Median |
AMIN |
Arithmetic Minimum of valid values (version info: 5.3_24.12) |
AMODE |
Arithmetic Mode |
AVARIANCE |
Arithmetic Variance |
AVARIANCEP |
Arithmetic Variance of Entire Population |
AVG |
Time Weighted Average |
AVGRAW |
Raw Time Weighted Average - ignoring the invalidity of values |
CALC |
User Defined Calculation. E.g. CALC(y*2) returns values doubled and |
CALCI |
Works like the CALC except in cases where there is change between zero and non-zero value, where it interpolates a new point to position where the value changes from zero to non-zero or vice versa. |
COUNT |
Count of Samples Within Period |
COUNTG |
Count of Good Samples Within Period |
COUNTI |
Count of Invalid Samples Within Period |
COUNTQ |
Count of Questionable Samples Within Period |
COUNTS |
Count of Substituted Samples Within Period |
CONVERT |
Converts Values to User Specified Unit. E.g. CONVERT(hp) can be used to |
CUMSUM |
Cumulative Sum |
CUMSUMTODOUBLE |
Cumulative Sum to Double Value |
DELTA |
Last Sample In Period minus First Sample In Period |
DEV |
Time Weighted Deviation |
DUR |
Duration = Period Length (changes only upon daylight savings or with month |
DURG |
Good Duration as a TimeSpan Within Period |
DURI |
Invalid Duration as a TimeSpan Within Period |
FIRST |
First Value of a Period |
FFT |
Fast Fourier Transform of input data |
HISTOGRAM |
Histogram of input data |
INTSEC |
Time Integral in Seconds |
INTMIN |
Time Integral in Minutes |
INTHOUR |
Time Integral in Hours |
LAST |
Last Value of a Period |
MAX |
Maximum Value of a Period, TimeStamp is the Value Time |
MAXPT |
Maximum Value of a Period, TimeStamp is the Period Time |
MIN |
Minimum Value of a Period, TimeStamp is the Value Time |
MINPT |
Minimum Value of a Period, TimeStamp is the Period Time |
OK |
Changes invalid values to valid |
OPTIME |
Operating Time. Requires a parameter, e.g. OPTIME10MIN(>5) calculates |
PERG |
Percent of Good Samples (0-1) |
PERI |
Percent of Invalid Samples (0-1) |
PLOT(xpixels,ypixels) |
Omit excess samples that the given the plot area resolution cannot display. Can also omit samples that are not needed when plotting linear lines between the samples and the result still looks the same. |
PLOTM(xpixels,ypixels) |
Plot with markers. Omit excess samples that the given the plot area resolution cannot display but do not omit physical samples that would be needed to plot the markers to the samples unless they are too close to each other. |
RANGE |
Maximum Value Within a Period minus Minimum Value Within |
SKIP |
Skip and select period values SKIP(initial_skip, value_skip) |
STABILITY |
Stability Graph - Fetches all the values in the time range, sorts them in descending order, and makes X-axis show the cumulative timespan based on how long each value was active. |
STARTUP |
Startup Count - requires a parameter. E.g. STARTUP5MIN(>5) calculates |
SUM |
Sum of Values Within a Period |
SUMRAW |
Raw Sum - Ignoring the Invalidity of Values |
SUMTODOUBLE |
Sum of Values Within a Period Calculated to Double - Use If There is a Risk |
VARIANCE |
Time Weighted Variance |
WHEN |
Conditional fetch of values. Returns requested values when given conditions |
Supported time periods
No period length |
The whole period between start time and end time is used. E.g. AVG return the |
TICKS, HUNDREDNANOSECONDS |
Hundred nanoseconds |
MICROSECOND, MICROSECONDS |
Microseconds |
MS, MSEC, MILLISECOND, MILLISECONDS |
Milliseconds |
S, SECOND, SECONDS |
Seconds |
MIN, MINUTE, MINUTES |
Minutes |
H, HOUR, HOURS |
Hours, local time |
H_UTC, HOUR_UTC,HOURS_UTC |
Hours, UTC time |
D, DAY, DAYS |
Days, local time |
D_UTC, DAY_UTC,DAYS_UTC |
Days, UTC time |
MON, MONTH, MONTHS |
Months, local time |
MON_UTC, MONTH_UTC, MONTHS_UTC |
Months, UTC time |
Y, YEAR, YEARS |
Years, local time |
Y_UTC, YEAR_UTC, YEARS_UTC |
Years, UTC time |
PL, PLEN, PERIODLENGTH |
Source data period lengths. E.g. if source data is AVG5MIN, AVG2PLEN produces |
Supported constants and functions in the CALC Filter
| y | Current y value |
| x | Current x value, in case of CALCI x may be the iterated or interpolated value |
| PI | pi |
| e | natural logarithmic base |
| nextx | next x value, at the end of the period it is the last x |
| nexty | next y value, at the end of the period it is the last y |
| prevy | previous y value, for the first value in result set this is the same as y |
| prevyz | previous y value, for the first value in result set this is zero |
| prevx | previous x value, for the first value in result set this is the same as x |
| prevcy | previous calculated y value (result of the calculation of previous values) |
| periodlength | period length in 100 nanosecond units |
| goodtime | time the value has not been invalid (representativeness affects too) |
| meantime | x-prevx |
| querystarx | (5.3 Dec-2025 and newer) query start x value (eg. start time if x axis is time) |
| queryendx | (5.3 Dec-2025 and newer) query end x value (eg. end time if x axis is time) |
When filter
The WHEN Filter can be used for conditional fetch of values. The filter returns the requested values
when conditions given as arguments are greater than zero. Syntax of the WHEN filter is below.
WHEN(Class=...;Property1=...;Property2=...; ...etc... PropertyN=...;xProperty=...;yProperty=...;
Filter=...)No argument is compulsory. There can be 0-N properties of the given class used as conditions.
Default value for "Class" is "ProcessHistory", which is used, if the "Class" argument is left empty.
Available classes are the same as the sources for a trend. Properties are the same as the properties
for the trend sources. E.g. a first property can be "Variable" and a second property can be "History"
for the "ProcessHistory" class. From 5.3 Dec-2025 and up you can also specify "xshift", to alter the x range the condition is fetched (eg. fetching from previous hour). Filter can be any valid filter operation.
In Example 1 clause returns the "CPU Total time" variable's values when the value is greater than 20.
WHEN(Class=ProcessHistory;Variable=SYS_CPU_TotalTime;XProperty=Time;YProperty=Value;xshift=00:00:00;Filter=
CALC(y>20))In Example 2 clause returns the same values as in Example 1, as the only difference is the lack of default values.
WHEN(Variable=SYS_CPU_TotalTime;Filter=CALC(y>20))In Example 3 clause returns time periods where Variable "BleacherState" has been 1 reduced with 20 seconds from both ends. The purpose of this example is to select "steady state" of the process, i.e. removing transition period at the start and end of the production period.
WHEN(Variable=BleacherState;Filter=CALCI(y==1 && (x-prevx)>seconds(20) && (nextx>x?(nextx-x)>seconds(20):1)))
In Example 4 clause returns the values of "float0" equipment property under the path "Plant1.Area1.Motor102" when the value is greater than 3.
WHEN(Class=EquipmentHistory;Path=Plant1.Area1.Motor102;Property=float0;Filter=CALC(y>3))Updated 9 months ago