Using VtrinCmd as the Export Tool
This document contains examples for exporting data with VtrinCmd.
For more information about connecting to a data source, connection types, credentials, and command parameters, see the VtrinCmd Tool documentation.
Parameters
| Command | Description |
|---|---|
| --connectionstring | Database Connection |
| --exportjson | Export JSON class data |
| --exportjsontreenode | Export JSON from TreeNode instance and other related data |
| --exporttofolder | Export individual TreeNodes recursively to target folder |
| --recursive | (with --exportjsontreenode) Export recursively the whole sub tree. |
| --outfile | Write output to a file |
Export the Root (or a specific ) TreeNode and Its Subtree into a Folder Hierarchy
Navigation items are described as TreeNode. To learn more about the concepts of TreeNodes and property bags, please visit: https://docs.abilityhistory.abb.com/docs/creating-an-application#/
VtrinCmd --connectionstring /path/to/your/data --exporttofolder .\target-folder-path\foldername --exportjsontreenode TreeNodeID
--recursive
JSON output: A complete folder hierarchy is generated under the specified output path, starting from either the root tree node (TreeNodeId: 00000000-0000-0000-0000-000000000000) or a selected tree node. Each folder represents a tree node and contains the exported JSON files for that node and all of its descendants. The export includes associated metadata, UI strings, and property bags.

The screenshot is for illustration purposes only. Please replace with your own values.
Export from the Root or a specific TreeNode
VtrinCmd --connectionstring /path/to/your/data --exportjsontreenode "Root-Node-ID" --recursive --outfile .\target-folder-path\filename.json
JSON output: A complete navigation tree starting from the root tree node (TreeNodeID: 00000000-0000-0000-0000-000000000000) or a specified tree node (TreeNodeID), including all descendant tree node instances. The export captures associated metadata, UI strings, and property bags.

The screenshot is for illustration purposes only. Please replace with your own values.
Equipment Model
Export All Equipment Models
VtrinCmd --connectionstring /path/to/your/data --exportjson Equipment --outfile .\target-folder-path\filename.json
JSON output: The base class and all of its derived classes, including their Id, Name, ClassName, and other related metadata fields.

The screenshot is for illustration purposes only. Please replace with your own values.
Export Multi-Selected Equipment Models
VtrinCmd --connectionstring /path/to/your/data --exportjson "Equipment[]:Mask|Equipment[]:Mask|Equipment[]:Mask"---outfile .\target-folder-path\filename.json
JSON output: The base class and the matching derived classes, including their Id, Name, ClassName, and other related metadata fields.

The screenshot is for illustration purposes only. Please replace with your own values.
Export a single Equipment Model
VtrinCmd --connectionstring /path/to/your/data --exportjson Equipment[]:Mask --outfile .\target-folder-path\filename.json
JSON output: The base class and the matching derived class, including its Id, Name, ClassName, and other related metadata fields.

The screenshot is for illustration purposes only. Please replace with your own values.
Equipment Property
Export EquipmentPropertyInfo for All Equipment Models
VtrinCmd --connectionstring /path/to/your/data --exportjson "EquipmentPropertyInfo" --outfile .\target-folder-path\filename.json
JSON output: All property definitions from the base equipment class and its derived models. Captures control tags, status fields, configuration parameters, and diagnostics. Each property entry contains metadata such as ID, display name, data type, default value, unit, historization settings, and a link to its corresponding equipment model via the Equipment reference.

The screenshot is for illustration purposes only. Please replace with your own values.
Export EquipmentPropertyInfo for Multi-selected Equipment Models
VtrinCmd --connectionstring /path/to/your/data --exportjson "EquipmentPropertyInfo[]:Equipment='Name1' OR Equipment='Name2' OR Equipment='Name3'" --outfile .\target-folder-path\filename.json
JSON output: Property definitions for the selected equipment models. Captures control tags, status fields, configuration parameters, and diagnostics across multiple models. Each property entry contains metadata such as ID, display name, data type, default value, unit, historization settings, and a link to its corresponding equipment model via the Equipment reference.

The screenshot is for illustration purposes only. Please replace with your own values.
Export EquipmentPropertyInfo for a Selected Equipment Model
VtrinCmd --connectionstring /path/to/your/data --exportjson "EquipmentPropertyInfo[]:Equipment='Name'" --outfile .\target-folder-path\filename.json
JSON output: All property definitions for the selected equipment model. Captures control tags, status fields, configuration parameters, and diagnostics. Each property entry contains metadata such as ID, display name, data type, default value, unit, historization settings, and a link to its corresponding equipment model via the Equipment reference.

The screenshot is for illustration purposes only. Please replace with your own values.
Equipment Instance
Export All Equipment Instances
VtrinCmd --connectionstring /path/to/your/data --exportjson Path --outfile .\target-folder-path\filename.json
JSON output: All instances defined under the base class. Each instance definition contains metadata describing fields such as Id, Name, DisplayName, and link back to its parent via the Equipment field.

The screenshot is for illustration purposes only. Please replace with your own values.
Export Selected Equipment Instances from Multiple Classes
VtrinCmd --connectionstring /path/to/your/data --exportjson ClassName1[properties]:Mask | ClassName2[properties]:Mask | ClassName3[properties]:Mask --outfile .\target-folder-path\filename.json
JSON output: Only equipment instances match the provided mask. Each instance contains metadata detailing fields such as Id, Name, DisplayName, and link back to its parent via the Equipment field.

The screenshot is for illustration purposes only. Please replace with your own values.
Export Instances from a Single Equipment Class
VtrinCmd --connectionstring /path/to/your/data --exportjson ClassName[]:Mask --outfile .\target-folder-path\filename.json
JSON output: All instances belonging to the specified equipment class/path. Each instance contains metadata detailing fields such as Id, Name, DisplayName, and link back to its parent via the Equipment field.

The screenshot is for illustration purposes only. Please replace with your own values.
Further Reading:
Learn more about VtrinCmd tool
Updated 10 days ago