Setting up archiving feature

This feature is only for Admin users

Important: This feature is not installed by default. If you’re a server admin, follow the steps below to enable it.

Installation

  • Packaged installer: Make sure the cpmPlusVtrinNetServerDashboardArchiver package is installed. It includes Chrome and the correct version of chromedriver.

  • Monolithic installer: You’ll need to manually download the correct chromedriver.exe that matches the version of Chrome installed on the server. Place the chromedriver.exe file in the same folder as Vtrin-NetServer.exe.

Configuration

Dashboard archiving can be customized using your Vtrin-NetServer.config file. Below is an example of the optional configuration section:

<configuration>
  <configSections>
    <!-- This configSections part is unfortunately neccessary because dotnet is validating this config file so it need to be told about this custom section schemas -->
    <sectionGroup name="webDriver">
      <section name="browser" type="System.Configuration.NameValueSectionHandler,System" />
      <section name="arguments" type="System.Configuration.NameValueSectionHandler,System" />
    </sectionGroup>
    <section name="dashboardArchivingConfig" type="System.Configuration.NameValueSectionHandler,System" />
  </configSections>
  <webDriver>
    <browser value="Chrome" />
    <arguments>
      <add value="headless" />
      <add value="ignore-certificate-errors" />
      <!-- <add value="auto-open-devtools-for-tabs" /> -->
      <!-- <add value="no-sandbox" /> -->
      <!-- <add value="disable-gpu" /> -->
      <!-- <add value="disable-extensions" /> -->
    </arguments>
  </webDriver>
  <dashboardArchivingConfig>
    <add name="Enabled" value="true" />
    <add name="SkipAuthCheck" value="false" />
    <add name="DefaultPaperSize" value="a3" />
    <add name="DefaultOrientation" value="landscape" />
    <add name="LoginSuccessIndicatorClassName" value="ABBMia_cTopBarUserName" />
    <add name="PrintReadyClassName" value="ABBMia_PrintReady" />
    <add name="UniqueNamingStyle" value="timestamp" /> <!-- timestamp or incremental -->
    <add name="LoginPageTimeout" value="6" />
    <add name="AuthCheckTimeout" value="11" />
    <add name="PrintPageTimeout" value="41" />
  </dashboardArchivingConfig>
  <!-- This is the Vtrin-NetServer example configuration file - you must edit this file to setup your server!	-->
  <!-- Vtrin-NetServer can be run either stand-alone or under Microsoft Internet Information Services (IIS) 	-->
  <!-- The address on the server will be formed like here: proto://computername[:port]/objectUri/datasourceUri 	-->
  <!-- Configure and copy this file to the directory the Vtrin-NetServer is installed and rename it to Vtrin-Netserver.config -->
  <!-- For more information, please see: https://abilityhistory.abb.com/wiki/index.php?title=Vtrin_Server_Configuration -->
  <appSettings>
    <!-- <add key="AccountQueryFilter" value="Domain='%COMPUTERNAME%'" />		     -->
    <!-- Win32_Account query WHERE clause - can be used for performance reasons to prevent Vtrin-NetServer from scanning complete domain for users. (if the security editor seems to freeze, you need to tune this one). -->
    <!-- <add key="ChangeSendDelay" value="500" />					     -->
    <!-- Time to wait in ms when event is triggered for further events to combine them into a single frame, set to zero to disable (will disable lag, but cause a lot of tcp ping pong with any larger amounts of events). -->
    <add key="CertificateName" value="vtrincert" />
....

All configuration values are optional—defaults are hardcoded. The feature will still function even without custom configuration.

For more advanced configuration and troubleshooting, refer to the technical documentation or contact support.


Did this page help you?