RTDB Driver Command Classes
This section describes command classes of RTDB Driver.
UpdateHistory
UpdateHistory is a command class to maintain timeseries history data, no base table. It is not stored anywhere. It lets user write, update, or delete values within a time range. Typical though process is:
- Choose what to update: a
Variable, or an equipmentPathandProperty. - Choose the time range (
StartTimetoEndTime) - Give the values for that time range (
StartTimeandEndTime) - Choose whether existing data may be overwritten.
- Submit the request. The history is updated
Parameters for procedure UpdateHistory:
| Name | Type | Description | Options/values |
|---|---|---|---|
| Variable | positive integer (uint32) | Destination variable to update. If set, Pathand Propertyare ignored | Variable's IDs |
| Path | GUID | Equipment instance. Used only when Variable is not set. | |
| Property | text | Name of the historized equipment property. Used with Path. | Only historized properties on the path's equipment class |
| History | positive integer (uint32) | Target history table | Defaults to the variable's TargetHistory or the equipment property's target history. Falls back to CurrentHistory |
| Scenario | positive integer (uint32) | Scenario to update | If set, the history name becomes <History>_SC<ScenarioId>_COMB |
| ItemType | integer (int32) | Kind of item being updated. | See ItemType table below. |
| CallMode | integer (int32) | How the user made the selection. | See CallMode table below. |
| Function | integer (int32) | Operation to run | 0 (none), 1 (get defaults), 2 (update), 3 (delete) |
| StartTime | DateTime | Start date time of the range. | UTC |
| EndTime | DateTime | End date time of the range | UTC |
| StartValue | Any value (object) | Value at the start time. | |
| EndValue | Any value (object) | Value at the end time. | |
| AllowOverwriting | boolean | Whether existing values may be overwritten | true or false |
| Comment | text | Comment stored with the update | The driver adds update information to it. |
ItemType
General purpose application should pass this as zero (if “caller” is Vtrin, a correct item type must be passed)
| Value | Name |
|---|---|
| 1 | Area |
| 2 | StackedArea |
| 6 | StackedColumn |
| 7 | StackedColumnOrdered |
| 8 | ClusteredColumn |
| 9 | Trend |
| 10 | Marker |
| 11 | XYScatter |
| 13 | LineRegression |
| 14 | ColumnWithHStatus |
| 15 | HStatus |
| 20 | Separator |
| 21 | Info |
| 22 | Gannt |
| 23 | GanntStatus |
| 24 | Limit |
CallMode
This should usually be passed as 1 (C_VirtualHistoryUpdate::m_kSpan). The other values are mainly for special purposes for Vtrin user interface.
The value 3 (m_kPoint) can be used for management purposes. It is a so called pointwise update that can be used for inserting or updating or deleting a single history sample. The application must itself be aware of the effects of history compression of the resulted operation.
| Value | Name |
|---|---|
| 0 | None |
| 1 | SingleCell |
| 2 | SingleColumn |
| 195 | SingleRow |
| 4 | SingleRowList |
| 9 | Free |
| 10 | MultiColumn |
| 203 | MultiRow |
| 204 | MultiRowList |
| 137 | FreeWithRowHighlight |
| 140 | MultiRowListWithHighlight |
Examples of UpdateHistory usage
var uh = driver.Classes["UpdateHistory"].Instances.Add();
uh["History"] = driver.Classes["History"].Instances.GetInstanceByName(historyName);
uh.SetRawPropertyValue("Variable", variableId);
uh.SetRawPropertyValue("StartValue", 13.0);
uh.SetRawPropertyValue("EndValue", 13.0);
uh.SetRawPropertyValue("CallMode", 1); // SingleCell
uh.SetRawPropertyValue("Function", 2); // update function
uh.SetRawPropertyValue("ItemType", 9); // Trend
uh.SetRawPropertyValue("StartTime", start);
uh.SetRawPropertyValue("EndTime", end);
uh.SetRawPropertyValue("Comment", "no comment");
uh.SetRawPropertyValue("AllowOverwriting", false);
uh.CommitChanges();POST https://myhost/odata/UpdateHistory
Content-Type: application/json
{
"Variable": <variable ID>,
"Function": 2,
"ItemType": 9,
"CallMode": 1,
"StartTime": "2025-01-01T00:00:00Z",
"EndTime": "2025-01-01T06:00:00Z",
"StartValue": 13.0,
"EndValue": 13.0,
"AllowOverwriting": false,
"Comment": "From OData"
}-- 1. Create a variable. The variable used in this example is "TestUpdateHistory".
-- 2. Save below SQL script to a file.
-- 3. Execute the sql-file using following command:
-- praocurr <RTDB location> --vtrin -script MyScript.sql
INSERT INTO UpdateHistory([TGT:Variable], ItemType, CallMode, Function, AllowOverwriting, [TGT:History], StartTime_UTC, EndTime_UTC, StartValue, EndValue) VALUES('TestUpdateHistory', 9, 1, 2, 1, 'CurrentHistory', { ts '2026-11-09 12:00:00.0000000'}, { ts '2026-11-09 13:00:00.0000000'}, '(Double)-1.5', '(Double)-1.5');
1. Create a variable
2. Right click it -> Send -> Trend
3. Highlight a range on the trend. This is for the time range, StartTime and EndTime
4. Choose the variable from the trend's list.
5. Assign StartValue and EndValue next to start's and end's date time.
6. Click commit
7. You may give comment and check "Allow overwriting the values after updating".
8. Click OK(Not available yet)Updated about 15 hours ago