TrailLog - Event Based History Archiving
ABB Ability™ History supports archiving of time series history data and events and storing the archived events in a separate log called TrailLog.
Storing Events for Analysis
Additional functionality related to TrailLog is that it is providing information for the dabase management to archive the history data that the event describes. This means that even if the event time period is going to be older that the retention time of the stored history data, the data is not removed from the database, but stored to separate Trail table. Trail table enable online analysis with the data even if it is beyond the length of the history table.
Browsing TrailLog Events
Engineering UI contains a list dashboard to browse TrailLog. With this dashboard you can also create new events and enable the archiving.
Attributes
Here we explain the meaning of the TrailLog event attributes.
Identification of the Event
| Field | Data Type | Description |
|---|---|---|
| Event Time | Timestamp | Time when the event was created. |
| Name | String | Name of the event. |
| Comment | String | Additional explanation of the event. |
Filtering for History Data Archiving
| Field | Data Type | Description |
|---|---|---|
| Start Time | Timestamp | Start time of the history period to archive. |
| End Time | Timestamp | End time of the history period to archive. |
| Process Path | Path ID | Archives all Variables and Equipment instances below the specified path. If null, includes all Variables and Equipment instances in the database. |
| Variable | Variable ID | Restricts archiving to a single Variable. |
| History | History Table ID | Restricts archiving to the specified history table. If not defined, all history tables and event logs are archived, if the table is enabled for archiving in the table configuration. |
Trigger Information (Optional)
| Field | Data Type | Description |
|---|---|---|
| Trigger Variable | Variable ID | Variable that triggered the TrailLog event. |
| Trigger Path | Path ID | ID of the Equipment instance that triggered the TrailLog event. |
| Trigger Type | String | Type of trigger, such as device failure. |
Miscellaneous
| Field | Data Type | Description |
|---|---|---|
| Expiration Time | Timestamp | Time when the event expires and its archived data can be deleted. |
| Row Status | Enum | Internal status of the archiving functionality. |
Updated 12 days ago