Plugin Development
This page is going through the basic steps to implement a plugin for the Notification Service.
Folder location
Plugins must be located in a sub-folder named Vtrin-NotificationServicePlugins[Version 5.3_25.04] (old name NotificationServicePlugins) in Vtrin folder. During installation, this folder should be automatically created and can be found in Vtrin folder.
Each plugin has its dedicated sub-folder with the same name. All dependency DLLs must be located here.
File naming
The main file of the plugin must be named with the prefix "NotificationServicePlugin_" for version 1 (e.g.: NotificationServicePlugin_Email.cs) or "NotificationServicePlugin2_" for version 2 (supported from 5.3_26.09).
Interfaces & parameters
Plugin 1
namespace ABB.Vtrin.NotificationService
{
public interface INotificationServicePlugin
{
void HandleMessage(string title, string content, string configurationstring);
}
}Plugin 2 (from 5.3_26.09)
namespace ABB.Vtrin.NotificationService
{
public interface INotificationServicePlugin2
{
void HandleMessage(System.Collections.Generic.IReadOnlyDictionary<string, object?> parameters);
}
}Parameters sent from Notification Service via plugin 2 interface:
| Key | Value |
|---|---|
| "title" | Title for the message |
| "content" | Content of the message |
| "configurationstring" |
Example
namespace ABB.Vtrin.NotificationService
{
public class ExamplePlugin : INotificationServicePlugin
{
private string mConfiguration;
public ExamplePlugin(string configuration)
{
mConfiguration = configuration;
}
public void HandleMessage(string title, string message, string configurationstring)
{
System.Console.WriteLine("Sending message to: " + configurationstring);
System.Console.WriteLine("Title: " + title);
System.Console.WriteLine("Message: " + message);
System.Console.WriteLine("Configuration: " + mConfiguration);
}
}
}For more comprehensive code example, please refer to Email and Azure WhatsApp plugins.
Updated 3 months ago