Periodical Schedulers
This display allows you to set up and define periodical schedulers. Howeverer, we recommend configuring these in the calculation settings as image below shows.

Periodical scheduler setting window in Calc Catalog display
| Property | Data type | Description |
|---|---|---|
| Name | String | Name of the periodical scheduler. |
| Execution Interval | Int32 | Provide interval of time for execution of the card. Must be positive number. |
| Execution Interval Unit | Enum | Interval unit on which to execute, e.g. second, minute, day. |
| Base Time | DateTime | How to align the execution times. For example, to run hourly at five seconds past, BaseTime should be 2000-01-01 00:00:05 and ExecutionInterval 1 hour. |
| Disabled | Boolean | This setting suspends the scheduler, not triggering any CalcTasks. |
Updated about 2 months ago
Did this page help you?