Task Triggers
This display allows you to monitor calculation task triggers. Disabling a trigger on this display, disables it in every calculation it is used. This in mind, possible changes should be done carefully.

Calculation task trigger settings can be configured in single calculation settings in Calc Catalog
| Property | Data type | Description |
|---|---|---|
| Task | Ref. CalcTask | Name of the calculation task. |
| Type | Enum | Name of the trigger used in calculation task as above image shows. See Trigger Settings for more information. |
| Mapping | Ref. CalcMapping | When calculation task is triggered by event, this column shows path/EquipmentModelName/Id. |
| Triggered By Task | Ref. CalcTask | When calculation task is triggered by other task, the triggering task name shows in this column. |
| Scheduler | Ref. CalcScheduler | Shows the scheduler name that is used in calculation task. If scheduler trigger is not used, column shows (None). |
| Event Properties | String | When event trigger is used in calculation task, this column shows the name of the triggering property/variable. |
| Disabled | Boolean | Disables the trigger shown in the TriggeredByTask / Scheduler / EventProperties column. E.g., if user disables 1min scheduler shown in "Scheduler" column, this setting disables the trigger in Calc Catalog. With this setting, all calculations using 1 min scheduler trigger will be disabled, meaning calculations will stop running. |
| Class Level Listener | Boolean | Shows event happening in Class property of any instance. Set to true, if you want to listen inserts in the table/class of your Mapping. |
| Polling Interval Secs | Double | Checks changes within defined period. Set the interval (seconds) to poll for new inserts in the specific table/class. The default and smallest permitted value is 5.0. If ClassLevelListener is set to true, but database-level events are not listened for the specific table/class, then polling is automatically used. For example, this is the case for the OpcEvent table. |
| Warnings | String | Warnings on calculations (not process). |
Updated 5 months ago
Did this page help you?