Equipment Model Bulk Load Tool - Reference
Detailed information
REFERENCE
Supported Types
| Type Supported | Example | Description |
|---|---|---|
| Boolean | True | Is either True or False. |
| Signed Byte | -10 | 8 bits integer. |
| Byte | 10 | 8 bits positive integer. |
| Short | -10 | 16 bits integer |
| Integer | 100 | 32 bits integer |
| Long | 12345678901234567890 | 64 bits integer |
| Float | 3.14 | 32 bits floating point number |
| Double | 3.141592653589 | 64 bits floating point number |
| DateTime | 00:00:01 | 1 second. Follow Standard TimeSpan format Notice: Make sure cell type is string. |
| String | hello | |
| TimeSpan | 00:00:40 |
Prefixing "Unsigned " to Short, Integer or Long define type as positive numbers. For array types, just append Array e.g. "Integer Array", then elements are listed in curly bracket e.g. {-2, -1, 0, 1, 2}.
Class Table
Class signature is Class : <class name> : <base class> . This will define a new class table which inherents all properties of <base class>. Inheretant is optional. Instead of Class, user can define AbstractClass, which is a Class with Abstract attribute set to true. AbstractClass can not be instantiated.
After the signature Class-table can virtually have any EquipmentPropertyInfo properties, e.g. ValueMin, ValueMax, DefaultValue, Attributes, TargetHistory, CompressionMethod, etc. Notice these headers are case sensitive.
TODO: Tell which properties will be generated automatically.
Instance Table
Instance table contain a list of instance of a class-table. All instance-table have following columns Parent, Name and class properties. Historized properties have extra columns to define their location over the network, such as Protocol, Server location, and Port. Supported Protocol are opc.tcp , opcda, and modbus. Following table describe which columns each protocol utilizes to define access path:
| Protocol | Columns | Description |
|---|---|---|
| opcda | Protocol, Server location, ProgId, ClsId, <historized property> | Access Path: Some columns can be empty, e.g. Server location, ClsId |
| opc.tcp | Protocol, Server location, Port, <historized property>, UaNamespace, UaIdType | Access Path:<Protocol>://<Server location>:<Port>///<historized property>;UaNamespace=<UaNamespace>;UaIdType=<UaIdType> |
| modbus | Protocol, Server location, Port, <historized property> | Access Path:<Protocol>://<Server location>/<Port>/<historized property> |
Parsing tool, ExcelPopulateEquipment.exe
ExcelPopulateEquipment.exe can generate a json file from a supported file, then the json file can be imported to a database.
ExcelPopulateEquipment.exe <supported file>
# supported file xlsx and xlsm works. CSV might work.Importing tool, VtrinCmd
VtrinCmd can import json file to database locally and remotely.
The syntax for import is:
VtrinCmd.exe -c <database location> -i <json file> [-u <user name>] [--dryrun] [--confirm] [--verbose] [-h]
#-c, --connectionstring Connection string for the driver.
#-u, --user User for the connection. (When using vault name prefix with *).
#-i, --importjson Import JSON data from a file(s). Multiple files separated with |
#-f, --force Forcefully remove conflicting instances
# --noreplace Do NOT replace/merge into existing class instances.
# --continueonerror Continue operation when an error occurs.
# --dryrun Perform a dry run - report changes but do not commit.
# --report Experimental (with --importjson option) Display detailed report.
# --confirm Same as dryrun + report with commit confirmed by the user.
# --verbose More console outputs.
#-h, --help Display help for using this tool.
# Example1: VtrinCmd.exe --confirm -c G:\rtdbdata -i G:\my.output.json
# Example2: VtrinCmd.exe --confirm -c wss://127.0.0.1/history -i G:\my.output.json -u <username>If report is enabled, user can see changes in the console:
+ means new.
* means modified.
in parantheses mean unmodified
Importing data from 'G:\WaterPumpSystem.xlsx.output.json'
#....
#....
Class: EquipmentPropertyInfo
(Manufacturer)
(Voltage)
+ Limit
Id: 5742d5e2-df28-4181-b07b-c943eb2d04f3
DisplayName: Limit
Equipment: Electrical device
Description: Voltage Limit
(Diameter)
* FlowFOOO
DisplayName: Flow -> FlowFOOO
(Level)
* VolumeFOO
DisplayName: Volume -> VolumeFOO
(Current power)
#......
#......
(Power state)
Class: DataAccessSource
({0, 0, /Path[Level]/ec36a8cf-d182-4301-bb09-2619813ee8ca|Example site.Water transfer system.Tank area.Source tank})
({0, 0, /Path[Level]/6d3c8426-85fa-4494-a96e-234bbbaf7275|Example site.Water transfer system.Tank area.Target tank})
Class: Path_Pipe
(Example site.Water transfer system.Flowback pipe)
(Example site.Water transfer system.Pipe)
#.......
#.......
Equipment 2 modified
EquipmentPropertyInfo 1 new 2 modified
--------------------------------------------------------------------------------
Total 1 new 4 modified (21 unchanged)
2020-06-17 23:19:56.1616402+03:00 (1) ABB.Vtrin.Util.JSON.Import: Total 0 instances imported
Commit changes (y/n)?Notice: It is possible to define access path under historized property by writing access path directly. E.g. under Level, a historized property of Tank has "opcda://custom_specs", then this value will be copied to access path.
Hints
Performance
Removing hyperlinks (as format) from cells improve processing time.
Updated about 1 month ago