Embedded C++ SDK onboarding
This is a getting-started guide for new users of embedded SDK (eSDK). Below are both Windows and Linux steps for obtaining, deploying and using eSDK in your solution. The general overview of eSDK can be found at Embedded C++ SDK.
Getting started on Windows
Installing Visual Studio
For running eSDK on the Windows platform, you need to use Visual Studio 2013 in eSDK version up to 5.1 and Visual Studio 2017 starting from version 5.2. Visual Studio 2019 can also be used instead of Visual Studio 2017 but the v141 C++ toolsets must be included to the installation.
-
Go to the Visual Studio page and download Visual Studio 2013 (recommended Professional or Enterprise, with latest updates)
-
During Visual Studio installation, no optional features
Accessing TFS and Embedded SDK source code
-
Open Visual Studio
-
Connect to TFS cpmPlus project:
- In Team Explorer, click on
Connect to Team Projectsicon, thenSelect Team Projects, then clickServers...button - Add
tfsa.abb.comserver (if not already present on the server list)- Click
Add...button - Fill in information as on the picture below and press
OK, and thenClose - TODO: IMAGE HERE
- Click
- Select tfsa.abb.com from the server list, then cpmPlus Team Project, and connect
- You might receive SSL connection error with description "The underlying connection was closed: Could not establish trust relationship for the SSL/TLS secure channel". It means that you are missing ABB Root CA certification authority, the easiest fix is to export this certificate from computer that already has it installed and import it to your destination computer:
- On your source computer, open command console and run
mmccommand, this will open Microsoft Management Console - Press
File, thenAdd/Remove Snap-in..., then add Certificates for current user: - TODO: IMAGE HERE
- Export ABB Root CA certificate to a file:
- TODO: IMAGE HERE
- On destination computer, also open Microsoft Management Console with
mmccommand - Import ABB Root CA from a file:
- TODO: IMAGE HERE
- On your source computer, open command console and run
- In Team Explorer, click on
-
In Source Code Explorer, map folder
$/cpmPlus/History/Main/eSDK/to a local folder of choice (in our examples it'sC:\eSDK) -
In Source Code Explorer, open solution
$/cpmPlus/History/Main/eSDK/Projects/cpmPlus_eSDK.sln. After opening it, there should be 4 projects accessible:cpmPlus_eSDK- source code for eSDK APIcpmPlus_eSDK_DemoApplication- sample application using eSDK APIcpmPlus_eSDK_Test- tests for eSDK APIMIA_Websocket- cross-platform wrappers for websocket communication, used for connecting to Vtrin (used internally by eSDK API)
Installing dependencies and building Embedded SDK library
- Install the OpenSSL libraries - latest 1.1 version for both Win32 and Win64
- During installation, select option to copy OpenSSL DLLs to Windows system directory
- To resolve includes in the project, run
makelink.bat, which is located inC:\eSDK\Projects\include(from command line as administrator) - In Visual Studio, set up project cpmPlus_eSDK as StartupProject
- Build the project in x86 mode
- Output files
cpmPlus_eSDK.libandMIA_Websocket.libare generated (inC:\eSDK\Projects\Win32\DebugorC:\eSDK\Projects\Win32\Releasefolder)
Creating a project that uses Embedded SDK library
-
Open Visual Studio, close previous solution and create a new project
-
TODO: IMAGE HERE
-
Open your
Project Properties, and then:- Set value of
Configurationbox to All Configurations- Go into
C/C++, then intoGeneral, and to the value ofAdditional Include Directoriesalso add C:\eSDK\Projects\include
- Go into
- Set value of
Configurationbox to Debug- Go into
C/C++, then intoCode Generation, and set the value ofRuntime Libraryto Multi-threaded Debug (/MTd) - Go into
Linker, then intoGeneral, and to the value ofAdditional Library Directoriesalso add:- C:\eSDK\Projects\Win32\Debug
- C:\eSDK\Projects\libs\openssl\lib
- Go into
Linker, then intoInput, and to the value ofAdditional Dependenciesalso add:- cpmPlus_eSDK.lib
- MIA_Websocket.lib
- libsslMTd.lib
- libcryptoMTd.lib
- Go into
- Set value of
Configurationbox to Release- Go into
C/C++, then intoCode Generation, and set the value ofRuntime Libraryto Multi-threaded DLL (/MD) - Go into
Linker, then intoGeneral, and to the value ofAdditional Library Directoriesalso add:- C:\eSDK\Projects\Win32\Release
- C:\eSDK\Projects\libs\openssl\lib
- Go into
Linker, then intoInput, and to the value ofAdditional Dependenciesalso add:- cpmPlus_eSDK.lib
- MIA_Websocket.lib
- libsslMT.lib
- libcryptoMT.lib
- Go into
- Set value of
-
Now you are ready to build and debug your project
-
In your application, to use eSDK functionality be sure to include following header files and Mia namespace:
#include "Mia_Driver.h" #include "Mia_Exception.h" #include "Mia_Base.h" #include "Mia_Equipment.h" #include "Mia_Device.h" using namespace ABB::Mia; -
To use eSDK, you also have to initialize the platform and connect to the edge:
static std::string g_Host = "wss://55.55.55.55/view/connectionstring.data"; static std::string g_Username = "username"; static std::string g_Password = "password"; int main() { ABB::Mia::G_PlatformInit(); ABB::Mia::C_MiaDriver driver(g_Host); try { std::cout << "[" << ABB::Mia::C_DateTime::M_S_Now() << "] [ INFO ]: Connecting to " << g_Host << std::endl; driver.M_Connect(g_Username, g_Password); } catch (ABB::Mia::C_Exception &ex) { std::cout << "[" << ABB::Mia::C_DateTime::M_S_Now() << "] [ ERROR ]: Failed to connect!! Reason: " << ex.M_ToString().c_str() << std::endl; return -1; } }
Getting started on Linux
Prerequisites
For running eSDK on the Linux platform, the minimal dependencies are:
- g++
- CMake (a project build system)
- Openssl development library
On debian-based systems with apt repository support, the below script can be used for installing dependencies:
#!/bin/sh
sudo apt-get update
sudo apt-get --yes install g++ build-essential openssl libssl-dev
Getting the code
The SDK code can be obtained from the TFS repository, with one of the following steps:
-
NFS synchronization
-
Using Eclipse and Team Explorer Everywhere plugin (the following steps were tested in Eclipse minimum version 4.0):
- Install Eclipse: https://www.eclipse.org/downloads/
- Install Team Explorer Everywhere plugin: https://marketplace.eclipse.org/content/team-explorer-everywhere
- Navigate to Windows → Preferences → Team → Team Fundation Server and enable "Accept untrusted SSL certificates" (see the picture below)
- TODO: IMAGE HERE
- Open Team Explorer perspective (Windows → Perspective)
- Use Connect to Team project for connecting to TFS server
- After a successful connection, the eSDK project should be accessible from Source Control view
-
tfs-cli command line interface (only if the basic-auth authentication or authentication token is enabled in the TFS repository)
Build and configuration
After obtaining the source code, navigate into the eSDK root folder, make the desired directory, where the library will be built into, and use cmake to build the project. An example of building the project can be found below. The recommended way is the out of source build:
cd eSDK
mkdir build
cd build
cmake ..
make
The following CMake options are available:
BUILD_TESTS=[ON/OFF]for building eSDK testsBUILD_DEMO=[ON/OFF]for building sample projectXCOMPILE=[ON/OFF]for cross-compilation
The options are used as follows:
cmake -DBUILD_TESTS=ON -DBUILD_DEMO=ON ..
The build options must be specified before the project path.
There are also two UI applications for more user-friendly cmake options editing:
- ccmake - Console gui app
- cmake-gui - Qt-based GUI, which allows for easy configuration of the build directory and build options. Example usage is shown in the picture below
TODO IMAGE HERE
Installation
Installation of Device API might be done with make install command. By default, targets are installed into /usr/local/ directory. The installation directory might be specified by setting cache variable during make generation:
cmake -DCMAKE_INSTALL_PREFIX=/path/to/install
Or, the whole installation might be relocated by using DESTDIR variable during install step:
make install DESTDIR=/path/to/install
In the case of setting DESTDIR targets will be put into path DESTDIR/CMAKE_INSTALL_PREFIX. For more information about DESTDIR see: https://cmake.org/cmake/help/v3.0/variable/CMAKE_INSTALL_PREFIX.html
After installation step, in the desired target directory will be 11 header files installed into include folder:
-
Mia_Base.h -
Mia_Device.h -
Mia_Driver.h -
Mia_Exception.h -
Mia_Equipment.h -
WS_Error.h -
WS_Socket.h -
WS_Util.h -
WS_Websocket.h -
Mia_Base_LINUX.h -
Mia_DriverBase.h
And two static libraries in the lib folder:
libcpmplus-sdk.alibMIA_Websocket.a
Cross compilation
Enabling cross-compilation is done by a flag XCOMPILE in CMake options. When cross-compilation is enabled, it is obligatory to specify CMAKE_CXX_COMPILER, CMAKE_C_COMPILER and CMAKE_SYSROOT cache variables. For example:
-DCMAKE_CXX_COMPILER=/path/to/g++compiler
Those variables might be set from cmake-gui by the Add Entry
After every change of the compilator, the CMake cache files MUST be deleted.
It can be done manually:
- Remove the
CMakeCache.txtfile - Remove the
CMakeFilesdirectory
It is also possible to use the python script cmake-clean.py with the build directory as an argument:
python cmake-clean.py <build directory>
Pay attention to the cmake command output, as it provides warning information if something is not set properly.
The compiled libraries would be in the <build_dir>/<target architecture>/lib folder, and executables in <build_dir>/<target architecture>/bin.
For example, in a 32-bit Linux system, the target libraries will be in: build/i686/lib
Running test and sample API usage
Test methods are using the gtest framework (bundled into the eSDK project). The source of the test is located in eSDK/SDK/src/MIA_Test/.
An example application using the eSDK API is located in eSDK/UseCases/
After successful compilation, there should be 2 Device API library files in the .../lib directory:
cpmplus-sdkwith Device API eSDKMIA_Websocketwith multi-platform websocket API
Also, there should be 2 executables in the .../bin directory:
cpmPlus_eSDK_Testwith the SDK testscpmPlus_DemoApplicationwith the example application
The test and demo code is the same for Linux and Windows, so you can also refer to the Windows part of this onboarding guide.
Writing CMake files for API usage
The following example will show how to make your own CMake file for your project to find, link and use the eSDK API. Add a file named CMakeLists.txt to your project root:
-
First, specify the used CMake version and desired C++, so your
CMakeLists.txtshould start like:#specify required cmake version cmake_minimum_required(VERSION 2.8) project(eSDK_App) #specify desired C++ standard set(CMAKE_CXX_STANDARD 11) -
Add the files with your code to the project files. You can set some name for them, or just add them in the
add_executablesection further on:#set files where your code is set(SOURCE_CODE Mia_BasicApplication.cpp) -
Specify, where to look for the eSDK API libraries. Let's assume that they are located in
/opt/eSDK/build/i686/lib. If the libraries are not found, cmake will show information about that fact, when generating the makefiles.#specify, where to look for eSDK compiled static libraries set(ESDK_LIB_DIR /opt/eSDK/build/i686/lib) #look for desired libraries find_library(ESDK_LIB NAMES cpmplus-sdk PATHS ${ESDK_LIB_DIR}) #Device SDK API find_library(MIA_WEBSOCKET_LIB NAMES MIA_Websocket PATHS ${ESDK_LIB_DIR}) #Websocket connection API required for eSDK API -
Include Device API headers and Websocket API headers:
#include Device API headers set(ESDK_HEADERS /opt/eSDK/SDK/src) #set directory where API source is located include_directories(${ESDK_HEADERS }/MIA_Driver) #include all headers in Device API directory include_directories(${ESDK_HEADERS }/MIA_Websocket) #include all headers in Websocket API directory -
Specify the build target for your application, and link against the required libraries:
#specify executable name add_executable(eSDK_BasicApp ${SOURCE_CODE}) #link against required libraries target_link_libraries(eSDK_BasicApp cpmplus-sdk MIA_Websocket pthread ssl crypto)
NoteIf the
make installfor eSDK was done, there is only need to include one folder:/path/to/installation/includeand all libraries are in/path/to/installation/libfolder, so following might be used instead of steps 3 and 4:include_directories(/path/to/installation/include) link_directories(/path/to/installation/lib)
In the end, the complete CMakeLists.txt file should look like:
#specify required cmake version
cmake_minimum_required(VERSION 2.8)
#specify desired C++ standard
set(CMAKE_CXX_STANDARD 11)
#specify, where to look for eSDK compiled static libraries
set(ESDK_LIB_DIR /opt/eSDK/build/i686/lib)
#look for desired libraries
find_library(ESDK_LIB NAMES cpmplus-sdk PATHS ${ESDK_LIB_DIR}) #Device SDK API
find_library(MIA_WEBSOCKET_LIB NAMES MIA_Websocket PATHS ${ESDK_LIB_DIR}) #Websocket connection API required for eSDK API
#set files where your code is
set(SOURCE_CODE Mia_BasicApplication.cpp)
#include Device API headers
set(ESDK_HEADERS /opt/eSDK/SDK/src) #set directory where API source is located
include_directories(${ESDK_HEADERS }/MIA_Driver) #include all headers in Device API directory
include_directories(${ESDK_HEADERS }/MIA_Websocket) #include all headers in Websocket API directory
#specify executable name
add_executable(eSDK_BasicApp ${SOURCE_CODE})
#link against required libraries
target_link_libraries(eSDK_BasicApp cpmplus-sdk MIA_Websocket pthread ssl crypto)It is recommended to have an out of source build with CMake. To do an out of source build, use the following commands from the directory where your CMakeLists.txt is located:
mkdir build
cd build
cmake ..
makeFor more examples of how to write CMake files, please refer to the cmake-tutorial.
Updated 6 months ago